Post Go back to editing

Help with LTC2943 – No I²C Response While Monitoring 14.8V 4S2P Li-Ion Battery

Category: Hardware
Product Number: LTC2943

Hello,

We are using the LTC2943 battery gas gauge IC to monitor a 14.8V nominal, 5.7Ah, 4S2P Li-Ion battery pack.

Our setup includes:

  • Sense resistor: 10 mΩ

  • M value: 4096 (based on IBAT/Qmax = 5.7 h)

However, when we try to communicate with the LTC2943 via I²C using an Aardvark I2C/SPI Host Adapter, we are not getting any response (no ACK or valid data from the device).

We’ve double-checked the connections and supply voltage, but still can't confirm whether the IC is functional or not.

Could you please help us with:

  1. Steps to confirm if the LTC2943 is alive and responding on the I²C bus.

  2. Any typical troubleshooting procedures or known issues when using the Aardvark tool with LTC2943.

  3. Any example I²C command sequences or required I²C timings for successful communication.

Any guidance would be greatly appreciated.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.