LT8491
Recommended for New Designs
The LT8491 is a buck-boost switching regulator battery charger that implements a constant-current constant-voltage (CCCV) charging profile used for most...
Datasheet
LT8491 on Analog.com
Hi,
I am attempting to use the LT8491 but I am not able to connect to the Chip over i2c. I have used a logic analyzer to see microcontroller is attempting to communicate with the LT8491 which is it. I performed a sweep of all addresses and have not had any response on the line from the LT8491. I know that the chip is working because I have a voltage reference from the output of AVDD. I was looking at the start up sequence and noticed that I2C is disabled upon startup but was unsure of how to check when it is enabled and if I should still be able read from the chip during all phases.
Any help is appreciated,
Thank you
Hi cwae ,
If you see the I2C traffic with a logic analyzer, then the bus is enabled.
Check these two things first:
1. SDA goes to SDA, SCL goes to SCL (check from datasheets, not from schematics symbols).
2. SDA and SCL lines have pull-up resistors (in range of 1k..10k).
Cheers, heke
Hi, Heke
I have double checked that the locations are right and then I used a logic analyzer to check the bus. I added a secondary slave to the bus, and I am able to see it but not able to see the LT8491.

I have gotten rid of all the components except for the required ones in the image below based on the block diagram. Would you have any thoughts on why I still can't see the chip?


Hi cwae ,
With the shown CA pin connection, the chip should ACK on 0x29H address. Wondering if you could capture the I2C waveform while addressing 0x29 << 1?
In the stripped down circuit you should not leave RT and MODE pins floating. Also VIN should probably be properly connected to a supply (or alternatively the EXTVCC) as some internal supplies are powered from it (also it may be that then the LDO33 pin undervoltage lock-out may disable I2C).
Kindly share your observations.
Cheers, heke
So, I tied mode to GND and RT to a 287K resistor to gnd. Then supplied voltage through VIN and looked at the output of LDO33. I tried with 2 different chips and got 6.4V and 1.4V as an output. Which is very weird. As for the waveform, I can see that there is no acknowledgement. The orange is clk and the red is data
0x29 << 1

0x29

Hi cwae ,
Cool. That LDO33 output is indeed weird. As it is an output of an LDO, it is mandatory to have a capacitor from the pin to ground, as otherwise the regulator is unstable. (if any chance, measure the LDO33 pin voltage using an oscilloscope. That may show if there is a stability issue). Place a 4.7uF or larger capacitor from the LDO33 to ground. Does it help?
Cheers, heke