Post Go back to editing

Understanding the configuration of operational sequences in the LPM state

Category: Software
Product Number: ADBMS6948

Hi

First, we need the source code to check the operating sequence in the LPM state.

(It is not related to ADBMS6815, ADBMS6830, or ADBMS6948, so please let me know the relevant reference source code)

Is it a method of defining the same sequence after sending a CMEN command to the LPM state and sending a CMHB command to enter the heartbeat state?

Or I would like to know if I should define the operation sequence without CMHB command transmission after the absolute time of 31 ms.