Post Go back to editing

Using the LTC681x library for systems based on either LTC6811-1 or ADBMS1818 ?

Category: Software
Product Number: LTC6811-1
Software Version: LTSketchbook LTC681x

We are currently using LTC6811-1 in our BMS system, the code based on LTC681x library. We are ready to build a new BMS system based on ADBMS1818 chip.

Can the latest downloaded LTC681x library be used for both systems: LTC6811-1 and ADBMS1818 -based?

Current LTSketchbook does not have the explicitly named ADBMS1818 library (at least I haven't found it) but I assume that LTC681x library is meant for both LTC6811 and also LTC6813 which is similar to ADBS1818, is it so?

I see in that file   #define IC_LTC6813 which is probably adding the extra features available in both LTC6813 and ADBMS1818 . If so, then would the toggling this define make the same library customized either for ADBMS1818 or for LTC6811-1 chip system?