MAX17300
Recommended for New Designs
The MAX17300–MAX17303/MAX17310–MAX17313 is a 24μA IQ stand-alone pack-side fuel gauge IC with protector and optional SHA-256 authentication for 1...
Datasheet
MAX17300 on Analog.com


I am using your fuel gauge to manage a LIION 3500mAh 1 cell battery, I configured the parameters using the configuration manager and the development kit.
In SBS compliant registers currents are reported correctly, but capacities are 4 times the value 4 mAh per LSB instead of 1 mAh.
I do not know what the problem is with the configuration.
I am attaching a screen shot of the configuration parameters, and the SBS related registers. The SBS registers in the development software convert capacity correctly, but the value of the register does not match 1 mAh/LSB as it should be.
What is the configuration issue ?
Thank you for the help.
Francisco Lira
Ph: 305-8225002