Post Go back to editing

Help with Charging Current Issue on Custom Board with MAX17332

Category: Hardware
Product Number: MAX17332

Hi,

I have an evaluation board and a custom board, both using the MAX17332 IC.

I used I2C to manually load the same custom configuration onto both boards. However, I’m encountering an issue:

  • On my custom board, the charging current is limited to around 60-80mA.
  • On the evaluation board, using the same configuration, it charges correctly at the desired current.

Could you provide tips on how to debug this issue or suggest where I should start looking?

Thank you,
Shai.