Hi, may i know the maximum number of daisy chain connection can be achieved in this device LTC6813? Thanks
LTC6813-1
Production
The LTC6813-1 is a multicell battery stack monitor that measures up to 18 series connected battery cells with a total measurement error of less than 2...
Datasheet
LTC6813-1 on Analog.com
Hi, may i know the maximum number of daisy chain connection can be achieved in this device LTC6813? Thanks
There is no limit to the maximum number of devices besides the bandwidth requirements of the system. For example, a 100 device daisy-chain will work but for a single 48bit read + PEC at 1mbps it will take (100 devices * 64bits * 1 second)/ 1mbit = 6.4ms.
Thanks, mvrablic