I want to use a 18 cell BMS and this is the BMS we chose. But I also want to measure current with ADBMS1818 BMS. How can I integrate a current meter into this circuit?
ADBMS1818
Recommended for New Designs
The ADBMS18181 is a multicell battery stack monitor that measures up to 18 series connected battery cells with a total measurement error of less than 3...
Datasheet
ADBMS1818 on Analog.com
I want to use a 18 cell BMS and this is the BMS we chose. But I also want to measure current with ADBMS1818 BMS. How can I integrate a current meter into this circuit?
It should support 80V (80/18s) and 100 Ampere. There is a 100 ampere limit for discharge, there is no limit for charge.
You can use ADBMS2949 or else you can use ADBMS2950B (which will need extra SPI port since it is not compatible with ADBMS1818) for coulomb counting. ADBMS2950B is the newest product with the newest features and simplified software design.
If you want all of the systems to work together and ADBMS6830B (18 cell IC which can balance all cells at once upto 300mA per cell) and ADBMS2950B (pack monitor for coulomb counting) + ADBMS6822 (isoSPI comm IC) would be the ideal combination.
You can use ADBMS2949 or else you can use ADBMS2950B (which will need extra SPI port since it is not compatible with ADBMS1818) for coulomb counting. ADBMS2950B is the newest product with the newest features and simplified software design.
If you want all of the systems to work together and ADBMS6830B (18 cell IC which can balance all cells at once upto 300mA per cell) and ADBMS2950B (pack monitor for coulomb counting) + ADBMS6822 (isoSPI comm IC) would be the ideal combination.