Post Go back to editing

How can I add a coulomb counter/current meter to ADBMS1818?

Category: Hardware
Product Number: ADBMS1818

I want to use a 18 cell BMS and this is the BMS we chose. But I also want to measure current with ADBMS1818 BMS. How can I integrate a current meter into this circuit?

Parents Reply Children
  • You can use ADBMS2949 or else you can use ADBMS2950B (which will need extra SPI port since it is not compatible with ADBMS1818) for coulomb counting. ADBMS2950B is the newest product with the newest features and simplified software design. 

    If you want all of the systems to work together and  ADBMS6830B (18 cell IC which can balance all cells at once upto 300mA per cell) and ADBMS2950B (pack monitor for coulomb counting) + ADBMS6822 (isoSPI comm IC) would be the ideal combination. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.