Post Go back to editing

MAX17303 Turning Off Discharge Transistors for 70ms Under 300mA Load

Category: Hardware
Product Number: MAX17303

Hello,

I’m using the MAX17303 fuel gauge on a custom board, and I’m experiencing an issue where the IC shuts off both discharge and charge transistors for approximately 70ms when I activate a sensor that draws 300mA.

This causes the microcontroller and other components to lose power, as the battery disconnection interrupts the supply.

I’ve checked the load and ensured it’s within reasonable limits, but I can’t seem to figure out why the MAX17303 is cutting off the discharge path.

Is there a specific register setting or configuration that I should adjust to prevent this behavior? How can I keep the discharge transistor from turning off under this load?

Any help would be greatly appreciated.

Thanks!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.