Post Go back to editing

Inquiry Regarding MAX17260 Fuel Gauge

Category: Datasheet/Specs
Product Number: MAX17260

Dear Analog Devices Support Team,

I am following up on the MAX1726X fuel gauge IC specifically. Based on the provided information about the "Capacity LSB SIZE" and "MAXIMUM VALUE," it appears that the valid capacity register info should be 8 bits wide (2^8 = 65535).

However, I would like to clarify if this is the case for all capacity registers in the MAX17260, or if there might be a larger 16-bit register where we only need to read the upper 8 bits for capacity information.

Your guidance on this matter will help ensure the correct implementation of the fuel gauge functionality in my design.

Thanks!