Post Go back to editing

MAX17055 Operating Current

Category: Hardware
Product Number: MAX17055

Dear Sir

I used DS91230+ and MAX17055 with 860mAh battery for 5 hours of no load operating current test

The starting capacity of the GUI battery is 97.094% (878mah) to 91.001% (876.5mah), Config reg: 0x1h = 2214. When THRM is not turned on, the operating current should not exceed 30uA.
The MAX17055 operating current read by the GUI consumes 1.5mA in 5 hours.
There is an electric meter mounted on the PCBA side to monitor the current consumption, and no large current is found to be drawn.
There is a big difference between GUI estimated current consumption and current. Is it a difference in REG settings or hardware?

There seems to be something else working

PS: Use DS91230+ and MAX17055 EVKIT with 860mah battery for 15 hours static measurement, GUI measurement from 99.656 (887.5mah) -> 99.180 (873mah)
Decrease 0.5% 4.5mA