Hi,
I'm using DC2026C with DC2259A to evaluate LTC6811-1 chip.
I have successfully written to DC2259A in the past (this includes the stock DC2259.ino file and modified script), but recently it began returning the following error:
I've tried closing all other programs, resetting the DC2026C board, and disconnecting DC2259A but none of it changes the error. The only solution was to download the Linduino library to my laptop and start fresh. I uploaded the DC2259A.ino file to the DC2026C. I thought 'great, it's working. Maybe there's a problem with my desktop setup.' Then I modified the script by just adding the line
Serial.print(BMS_IC[current_ic].cells.c_codes[i]*0.0001,4);in the loop. The same error returned. I tried uploaded the stock DC2259A.ino file and the error persisted.
Are there any ADI staff that can assist with this issue? I am also available for a video call to troubleshoot if necessary. Thanks in advance.f