Post Go back to editing

Two MAX17703 on one PCB for one battery each do not work

Category: Hardware
Product Number: MAX17703

Dears,

I have one PCB with two MAX17703 for one battery each (Lipo 6s/12Ah). If I connect only battery 1 and switch on the charging power supply (30V/30A), it works fine. If I connect only battery 2 and switch on the charger, it also works. But if I connect both batteries and switch on the charger, only the first battery charges. I have built 4 boards and all of them have the same issue.
The only thing the two MAX17703 share is the charging power supply, everything else is separate.

I really have no idea why it doesn't work. Can anyone help me or give me a tip?

Thank you very much.
Doenis

Parents Reply Children
No Data