We need to connect the MAX77650 to the Audio DSP, which is powered from the SIMO line(V Sbb0 = 1.2 V).
When the battery is first connected, MAX77650 is in STANDBY state and does not generate voltage to SIMO (V Sbb0 = 0 V).
That means, we cannot turn on Audio DSP. We need to wake up the MAX77650 chip from sleep.
We also cannot install a button or slide switch to nEN.
So, how we can solve this problem?