Hi Team,
We designed a power transmitter using LTC4125. The resonant freqency of charger is set to 203KHz. Also the charging current is 50mA. We are facing some issues with the charger. The charger is detecting reciever even in the absence of reciever and it is delivering power continuously. It is observing that the transmitter is not at all searching for the reciever. When ever we power up the trasmitter device , it is delivering power continuously. we have provided a status LED to indicate the reciever detection. It also turns on when we power up the device. We are observing some heating also in the board. May i know the possible reasons for this Issue. Also please let me know your suggestions