Post Go back to editing

LTC6813 communication issue - Linduino DC2792B

Thread Summary

The user encountered communication issues with an LTC6813 setup measuring 12 cells in series using a Linduino and DC2792B over isoSPI. The problem was resolved by adjusting the resistor values to R1=1.4kohm and R2=604ohm, as recommended for optimal performance. The user also confirmed that ISOMD was tied to VReg and that the 6813 was powered directly from the cells with 44V on V+.
AI Generated Content
Category: Hardware
Product Number: LTC6813-1

Hi

I am working on a project trying to communicate with a LTC6813 setup measuring 6 cells in series. I have a linduino and DC2792B to communicate via isoSPI.I am also using the arduino libraries provided by analogue devices inc. Unfortunately I am not getting communications with the LTC6813.

The battery comes from a vehicle that is made up of multiple modules. They use isoSPI to communicate as the BMS has 6820 deployed. I am trying to communicate with the final module which has a 2 wire comms connection.

Are there any debugs I could try to try and get comms. I have checked pins and scoped the isoSPI line and all seems correct.

Many thanks

Jack