Post Go back to editing

LiFePo4 configuration for MAX17301

Thread Summary

The user sought a configuration profile for a LiFePO4 (1S) battery with a 10Ah capacity (2.6-3.6V) for the MAX17301XEVKIT. The support engineer provided an INI file with default settings suitable for LiFePO4 batteries, which can be loaded into the EVKIT GUI and further configured using the wizard.
AI Generated Content
Category: Software
Product Number: MAX17301
Software Version: MAX17301XEVKIT software 1.0.16.0

Hi,

we would like to use the MAX17301XEVKIT development kit and the software for this kit to generate the basic configuration for the fuel gauge in our product. We are using a LiFePo4(1S) battery with a capacity of 10Ah (voltages in the range of 2.6-3.6V).
Unfortunately, the software does not allow to lower the voltages to levels for this type of battery.
There is a note in the software that we should contact the manufacturer if we use a LiFePo4 battery.

Hence my question, can we download or get an additional profile or settings for this type of battery?

Best Regards,

Paweł

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.