Post Go back to editing

Can MAX77789 D+/D- Pins be Left Open if only USB Type-C CC Detection is Required?

Category: Hardware
Product Number: MAX77789

I would like to avoid using the D+/D- pins since BC1.2 and proprietary standard support is not required, and the D+/D- pins are already being used for data. I would also like to avoid using a USB Mux as suggested by the datasheet.

Is it possible to leave these pins open on the MAX77789?

Thank you,

Lukas

Edit Notes

tagged
[edited by: GenevaCooper at 4:24 PM (GMT -5) on 5 Feb 2024]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.