Post Go back to editing

MAX17211 Accuracy

Category: Software
Product Number: MAX17211
Software Version: 2.0.8.0

Hello,

    This is Gavin from china,I got a quetion about MAX17211.

A single 4.2V lithium battery uses MAX17211 as a fuel gauge, which MAX17211 charge and discharge at room temperature and high temperature, and the SOC accuracy is very good, but at a low temperature of -40 degrees, the discharge current is 5A, and when the battery voltage drops to the 2.5V (protection threshold), the power is still 15%.

How can I fix this? thanks you very much!



tagged
[edited by: GenevaCooper at 8:27 PM (GMT -5) on 20 Nov 2023]