Post Go back to editing

[MAX77789] STAT2 pin default setting to charger detection done indication

Category: Hardware
Product Number: MAX77789

Hey,

I went through the datasheet for MAX77789 and I'm interested in using this IC for a new design  that also has an active USB 2.0 datapath. In the datasheet application example the STAT2 pin is used for controlling a MUX for the data lines, but as I understand the default mode for this is fault indication, and the reset value of the STAT2_USAGE is 0b00 which is the FAULT indication mode.

My questions are:

- Given that an I2C write transaction has to be done in order to properly control the data lines MUX, I don't see how an initial bootstrap would work, where the pin operates as a fault indicator. How this would look like in  terms of timings? I haven't found info on timing when the I2C interface is available for transactions.

- Is there an option to program a non-volatile memory to set the defaults, so even in case of complete loss of power the default setting for STAT2 is that it indicates charger detection done?

- Does this device support operating without a battery, only from VBUS?

- Is there any alternative AD product that has similar functionality, but has a dedicated pin for signaling charger detection complete that can be used for driving a data lines MUX without any supervision?

Thanks & BR,

Ferenc

Edit Notes

tagged
[edited by: GenevaCooper at 10:57 PM (GMT -5) on 29 Nov 2023]
Parents Reply Children
No Data