Post Go back to editing

Labview with LTC6811 BMS Daisy Chain Issues

Category: Software
Product Number: ltc6811-1
Software Version: Labview 2019

Hi, im trying to build a BMS by using 2 ltc6811-1 boards and daisy chaining them together. I am confused as to how the isoSPI works. For the first board which is connected to my controller, i am using the 14-ribbon SPI. For the connection of the bottom board to the top board i am using the RJ45 cable provided. In my Labview program, i am unsure of how to wake up the second board. My current program is able to read up to 12 cells but I am looking to further expand its capabilities. From what i can understand, the isoSPI port takes 600us to wake up and be at the ready state. I would have to wake up the isoSPI port before sending the read configuration command? x0002. 

Parents
  • I am still having issues with my program. I have calculated my Twakeup time to be 0.008s as my serial communication frequency is 20kHz.  My current transition state is 1) Wake up IsoSPI 2) Read Config 3) Set Config 4) Start Cell 5) Read Group A 6) Read Group B 7) Read Group C 8) Read Group D 9) Clear Register. I came across a LTC6820. From what i understand it seems that its able to solve my isoSPI issue without me having to change my current program which was monitoring 12 cells before. Would buying a LTC6820 help me to solve my problem?

Reply
  • I am still having issues with my program. I have calculated my Twakeup time to be 0.008s as my serial communication frequency is 20kHz.  My current transition state is 1) Wake up IsoSPI 2) Read Config 3) Set Config 4) Start Cell 5) Read Group A 6) Read Group B 7) Read Group C 8) Read Group D 9) Clear Register. I came across a LTC6820. From what i understand it seems that its able to solve my isoSPI issue without me having to change my current program which was monitoring 12 cells before. Would buying a LTC6820 help me to solve my problem?

Children
No Data