Do you have an equivalent of the MAX77960/77961/77962 for 1 1S battery?
I want to use the MAX77958 Controller, but the application is for a 1S battery.
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
MAX77960
Production
The MAX77960/MAX77961 are high-performance wide-input 3A (MAX77960)/6A (MAX77961) buck-boost chargers with Smart Power Selectorâ„¢ and operate as a reverse...
Datasheet
MAX77960 on Analog.com
MAX77958
Production
The MAX77958 is a robust solution for USB Type-C CC detection and power delivery (PD) protocol implementation. It detects connected accessories or devices...
Datasheet
MAX77958 on Analog.com
Do you have an equivalent of the MAX77960/77961/77962 for 1 1S battery?
I want to use the MAX77958 Controller, but the application is for a 1S battery.