Hi,
After battery replacement, I can't wake up the MAX17301 with pushbutton.
Only charging wake up them.
How I can wake up with push button after battery replacement ?
In attachement : my config file.
Thanks,
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
MAX1301
Production
The MAX1300/MAX1301 multirange, low-power, 16-bit, successive-approximation, analog-to-digital converters (ADCs) operate from a single +5V supply and achieve...
Datasheet
MAX1301 on Analog.com
MAX17301
Recommended for New Designs
The MAX17300–MAX17303/MAX17310–MAX17313 is a 24μA IQ stand-alone pack-side fuel gauge IC with protector and optional SHA-256 authentication for 1...
Datasheet
MAX17301 on Analog.com
Hi,
After battery replacement, I can't wake up the MAX17301 with pushbutton.
Only charging wake up them.
How I can wake up with push button after battery replacement ?
In attachement : my config file.
Thanks,
Config fie :
Device = MAX1730x Target DevName: <= 0x4067 Title = EVKIT Configurator Profile Generated on 2023/05/30 11:35:05 0x180 = 0x0000 //nXTable0 Register 0x181 = 0x0000 //nXTable1 Register 0x182 = 0x0000 //nXTable2 Register 0x183 = 0x0000 //nXTable3 Register 0x184 = 0x0000 //nXTable4 Register 0x185 = 0x0000 //nXTable5 Register 0x186 = 0x0000 //nXTable6 Register 0x187 = 0x0000 //nXTable7 Register 0x188 = 0x0000 //nXTable8 Register 0x189 = 0x0000 //nXTable9 Register 0x18A = 0x0000 //nXTable10 Register 0x18B = 0x0000 //nXTable11 Register 0x18C = 0x0000 //nVAlrtTh Register 0x18D = 0x0000 //nTAlrtTh Register 0x18E = 0x0000 //nIAlrtTh Register 0x18F = 0x0000 //nSAlrtTh Register 0x190 = 0x0000 //nOCVTable0 Register 0x191 = 0x0000 //nOCVTable1 Register 0x192 = 0x0000 //nOCVTable2 Register 0x193 = 0x0000 //nOCVTable3 Register 0x194 = 0x0000 //nOCVTable4 Register 0x195 = 0x0000 //nOCVTable5 Register 0x196 = 0x0000 //nOCVTable6 Register 0x197 = 0x0000 //nOCVTable7 Register 0x198 = 0x0000 //nOCVTable8 Register 0x199 = 0x0000 //nOCVTable9 Register 0x19A = 0x0000 //nOCVTable10 Register 0x19B = 0x0000 //nOCVTable11 Register 0x19C = 0x0000 //nIChgTerm Register 0x19D = 0x0000 //nFilterCfg Register 0x19E = 0xA561 //nVEmpty Register 0x19F = 0x0000 //nLearnCfg Register 0x1A0 = 0x1080 //nQRTable00 Register 0x1A1 = 0x2043 //nQRTable10 Register 0x1A2 = 0x078C //nQRTable20 Register 0x1A3 = 0x0880 //nQRTable30 Register 0x1A4 = 0x0000 //nCycles Register 0x1A5 = 0x1A90 //nFullCapNom Register 0x1A6 = 0x08CC //nRComp0 Register 0x1A7 = 0x223E //nTempCo Register 0x1A8 = 0x0000 //nBattStatus Register 0x1A9 = 0x1A90 //nFullCapRep Register 0x1AA = 0x0000 //nVoltTemp Register 0x1AB = 0x0000 //nMaxMinCurr Register 0x1AC = 0x0000 //nMaxMinVolt Register 0x1AD = 0x0000 //nMaxMinTemp Register 0x1AE = 0x0000 //nFullCapFltr Register 0x1AF = 0x0000 //nTimerH Register 0x1B0 = 0x2615 //nCONFIG Register 0x1B1 = 0x0204 //nRippleCfg Register 0x1B2 = 0x0000 //nMiscCFG Register 0x1B3 = 0x0000 //nDesignCap Register 0x1B4 = 0x0000 //nSBSCFG Register 0x1B5 = 0x1901 //nPACKCFG Register 0x1B6 = 0x083B //nRelaxCFG Register 0x1B7 = 0x2241 //nConvgCFG Register 0x1B8 = 0x0A20 //nNVCFG0 Register 0x1B9 = 0x0986 //nNVCFG1 Register 0x1BA = 0xFE0A //nNVCFG2 Register 0x1BB = 0x8909 //nHibCFG Register 0x1BC = 0xA426 //nROMID0 Register 0x1BD = 0x99D8 //nROMID1 Register 0x1BE = 0x0050 //nROMID2 Register 0x1BF = 0x8800 //nROMID3 Register 0x1C0 = 0x8480 //nPReserved0 Register 0x1C1 = 0x8780 //nPReserved1 Register 0x1C2 = 0x0000 //nPReserved2 Register 0x1C3 = 0x9D80 //nPReserved3 Register 0x1C4 = 0x0000 //nRGain Register 0x1C5 = 0x0000 //nPackResistance Register 0x1C6 = 0x0000 //nFullSOCThr Register 0x1C7 = 0x0000 //nTTFCFG Register 0x1C8 = 0x4000 //nCGAIN Register 0x1C9 = 0x0035 //nTCurve Register 0x1CA = 0xF284 //nThermcfg Register 0x1CB = 0x18E8 //nTOFF Register 0x1CC = 0x0000 //nManfctrName Register 0x1CD = 0x0000 //nManfctrName1 Register 0x1CE = 0x0000 //nManfctrName2 Register 0x1CF = 0x03E8 //nRSense Register 0x1D0 = 0x648C //nVPrtTh1 Register 0x1D1 = 0x3700 //nTPrtTh1 Register 0x1D2 = 0x5528 //nTPrtTh3 Register 0x1D3 = 0x4BB5 //nIPrtTh1 Register 0x1D4 = 0xDC00 //nVPrtTh2 Register 0x1D5 = 0x2D0A //nTPrtTh2 Register 0x1D6 = 0x7A28 //nProtMiscTh Register 0x1D7 = 0x0A00 //nProtCfg Register 0x1D8 = 0x644B //nJEITAC Register 0x1D9 = 0x0059 //nJEITAV Register 0x1DA = 0x5054 //nJEITACfg Register 0x1DB = 0xC884 //nStepChg Register 0x1DC = 0xAB3D //nDelayCfg Register 0x1DD = 0x0EAF //nODSCTh Register 0x1DE = 0x4355 //nODSCCfg Register 0x1DF = 0x00E5 //nCheckSum Register 0x1E0 = 0x0000 //nDPLimit Register 0x1E1 = 0x0000 //nScOcvLim Register 0x1E2 = 0x0000 //nAgeFcCfg Register 0x1E3 = 0xA5B9 //nDesignVoltage Register 0x1E4 = 0x0000 //nPackCfg2 Register 0x1E5 = 0x0000 //nRFastVShdn Register 0x1E6 = 0x0000 //nManfctrDate Register 0x1E7 = 0x0000 //nFirstUsed Register 0x1E8 = 0x0000 //nSerialNumber0 Register 0x1E9 = 0x0000 //nSerialNumber1 Register 0x1EA = 0x0000 //nSerialNumber2 Register 0x1EB = 0x0000 //nDeviceName0 Register 0x1EC = 0x0000 //nDeviceName1 Register 0x1ED = 0x0000 //nDeviceName2 Register 0x1EE = 0x0000 //nDeviceName3 Register 0x1EF = 0x0000 //nDeviceName4 Register