Hi,
I'd like to know what the red color of CFGR0 mean after READ CONFIG on LTC6804/LTC6811 MULTICELL MONITOR V05.3 GUI.
Does it indicate something bad or caution? It seems red all the time.

LTC6811-1
Production
The LTC6811 is a multicell battery stack monitor that measures up to 12 series connected battery cells with a total measurement error of less than 1.2mV...
Datasheet
LTC6811-1 on Analog.com
Hi,
I'd like to know what the red color of CFGR0 mean after READ CONFIG on LTC6804/LTC6811 MULTICELL MONITOR V05.3 GUI.
Does it indicate something bad or caution? It seems red all the time.

This red indication says there's a mismatch between what's written and what's read back from the CFG register of the device. You were writing 0xF8 into the CFG register of the device but what you read back is 0xD8 which is not the same as what's written.
The CFGR0 bytes consist of GPIOx bitfields which generally turn on/off the Internal Pull Down based on what's being written into it. But while reading back the same register, it checks what's the logic level on the pin and accordingly returns the result.
I guess there's a GPIO Pullup resistor missing on the GPIO3 Pin on the demo board. Please confirm if your components in the board match the demo board schematics.
Hi SideshS,
Thank you for your support. I understood the behavior clearly.
Regards,
Hi Jeam,
Can I know where you download the GUI for V05.3 GUI? I can't seem to find it on the Analog Device webpage
Hi cyongjed,
I cdould use V05.3 with two files. I downloaded them from these URL.
QuikEval
www.analog.com/.../dc2026c.html
COM Module
ez.analog.com/.../q1-cannot-load-com-module
Regards,
Hi cyongjed,
I cdould use V05.3 with two files. I downloaded them from these URL.
QuikEval
www.analog.com/.../dc2026c.html
COM Module
ez.analog.com/.../q1-cannot-load-com-module
Regards,