Post Go back to editing

Maximum number of LTC6801 in a daisy chain

Category: Hardware
Product Number: LTC6801

Hello, 
I am working on a design with the LTC6801 and there are >10 of these ICs in series. The chip requires up to a 40kHz pulse and each chip is transformer isolated. I am seeing the pulse get distorted after the 6th-7th IC. Is there a maximum number of these chips I can connect in series?

  • As a follow-up which might help us come to a solution, is the Frequency Match Detect Circuitry that is internal to the chip dependent on the phase of EIN and SIN? For example, as the number of chips in the daisy chain increase, there bound to be a phase mismatch between EIN and SIN. Does the Frequency Match Detect Circuitry get thrown off by this mismatch?