Hello,
My customer use LTC6813-1 in their system and 15 Cell is used only.
And at thehis system, they found 15S BMS dara error.
As the spec. in Datasheet, max. value of TME in Normal mode is Max. ±3.3mV.
But when they measured Cell1 & Cell15, Cell 1 is 4.4mV and Cell 15 is 6.6mV.
Other cells are in ±3.3mV.
Q1) Would you share your opinions why value of Cell 1 & Cell 15 are over Max. ±3.3mV which value is a spec. in datasheet?
Q2) Would you check their schematic in 4 page of attached file?
Q3) Would you check a test procedure and test result in 2, 3 Page of attached file?
Please advise me.
Regards,
Se-woong