Hello to ADI support team ,
I have some questions according LTC6811-1 , 2 units connection on the same board for 20S configuration .
1. Coupling Configuration from Data sheet there is 2 options : A - CMC + Capacitors , B - CMC + Signal Transformer .
1.1. If my IC's (LTC6811-1) on the same board is it sufficient make signal coupling through the simplest form through Capacitors ?
2. Can I use SPI Communication through the bottom IC directly without LTC6820 ?
3. Can I use I2C directly to the Controller from the bottom LTC6811-1 ?
4. What is the main reason data sheet introduce Controller Connection with LTC6811-1 through LTC6820 ?
5. Do you have dedicated guide for cascade connection for high capacity packs ?
B.R
Alexander Burtakov