LTC6810-1
Production
The LTC6810 is a multicell battery stack monitor. The LTC6810 measures up to 6 series-connected battery cells with a total measurement error of less than...
Datasheet
LTC6810-1 on Analog.com
Hi, im working on my final MSc Project wich is a BMS.
It is based on an LTC6810, wich in my case i used an DC2515B and an DC1941D isoSPI interface.
So far so good, i´ve tested the system using the DC2515b code on an arduino UNO and it all works well, the problem arrises when using an ESP32, wich i cant seem to make it communicate with the DC2515b.
Im thinking that the problem is with the SPI programming...can anyone help me with this?
Thank you in advance