Post Go back to editing

ESP32 SPI communication with LTC6810( DC2515B).

Category: Software

Hi, im working on my final MSc Project wich is a BMS.

It is based on an LTC6810, wich in my case i used an DC2515B and an DC1941D isoSPI interface.

So far so good, i´ve tested the system using the DC2515b code on an arduino UNO and it all works well, the problem arrises when using an ESP32, wich i cant seem to make it communicate with the DC2515b.

Im thinking that the problem is with the SPI programming...can anyone help me with this?

Thank you in advance Slight smile

Parents Reply Children