How can it be estimated at different charging currents as to what would be the drop across VCC-VBAT?
The data sheet mentions at two currents (90 and 10mA).
LTC4065L
Production
The LTC4065L is a complete constant-current/constant-voltage linear charger for single-cell lithium-ion batteries. Its small size and ability to accurately...
Datasheet
LTC4065L on Analog.com
How can it be estimated at different charging currents as to what would be the drop across VCC-VBAT?
The data sheet mentions at two currents (90 and 10mA).
Please help me provide a meaningful answer to your question by providing a little more info on the 10mA/90mA currents. I do not see references in the datasheet to 10/90mA currents, but I do see references to 10%/90% of programmed charge current. Might you be referring to the spec on p. 3 of the datasheet for ΔVUVCL ? I apologize if I have misinterpreted your request.
The data sheet references to 10%/90% of programmed charge current, the Rprog is 2K, which means that the charging current is set to around 100mA, so I came up with the number of 10mA and 90mA.
Our charging current is at 40mA. So the question is with the numbers given for ΔVUVCL : how will it vary for different charging currents? At the minimum it should be related to the RDS on of the series MOSFET as shown in graph Power FET On Resistance vs Temperature on page 5.
So will a lower charging current allow me to use a VCC of closer to 3.75Volts ?
I think the best you can do is to interpolate the 10% and 90% figures and arrive at a figure for 40mA that way. Note that the ΔVUVCL figure at 10% and 90% are typical, with min and max specified at 25°C. The typical figures work out to ΔVUVCL=148mV for a charging current of 40mA.