Hello to community
I use a Arduino uno with ft232 and a mine board with ltc6804-1, when a upload from sketchbook the DC1894 to my Arduino uno i can to connect with LTC6804-1 and read the cell voltage and etc from serial port via of Arduino IDE. When from sketchbook upload to my Arduino the DC590B i have comunication between arduino uno and serial port by take the message HELLO any time press the reset buton but when i tray to connect with quikevalK114 GUI i take the message USB TO SERIAL CONTRLLER ITS NOT CONNECTED that mean i have connection between usb and arduino when use sketchbook DC1894 and DC590B but not connection between GUI and Arduino.What i do wrong? i download and install GUI from AD website (DC2026 software), i want to use ltc6804/ltc68011 multicell monitor. Thanks