Hi,
I'm not seeing the intended output voltage from the VOUT1 (Buck-Boost Regulator) on my LTC3567. The schematic is attached. It's a pretty vanilla application, very similar to the example applications in the datasheet. Could I get a quick verification that the schematic is at least correct?
I've already gone through my board and checked for shorts and opens and everything seems to be physically connected according to the schematic.I currently don't have a battery attached because I'm still going through board bring up.
VOUT1 goes to a current sense resistor (+3.3V_SNS) and the +3.3V rail is on the other side of that current sense resistor, which the FB1 pin is biased from.
I temporarily tied the EN1 pin to VOUT (which I've measured to be 3.6V) to enable the buck-boost converter, since I don't currently have a battery attached it seems the default setting is for the VOUT1 to be OFF according to the default 0xFF00 value in the control register.
The datasheet mentions that "the switching regulator delivers power until the CLPROG pin reaches 1.188V." I measured the voltage at the CLPROG and it was only at 0.3V
Any help for a sanity check would be appreciated. Thanks!