Post Go back to editing

LTC6813 Cell Balancing questions

Thread Summary

The user inquired about the initialization sequence for cell balancing in the LTC6813, including sample code, PWM duty cycle configuration, discharge timer for balancing up to 10mV over 12 hours, and the impact on adjacent cells. The final answer indicated that the question was addressed in direct main support. The user observed a 2V drop across the balancing resistor for the targeted cell and a 17-18mV drop for the adjacent cell when cell balancing was enabled.
AI Generated Content

Hi,

We are implementing cell balancing using LTC6813. We have the following questions:

  • What is the initialization sequence for Cell balancing in LTC 6813? Where can I get sample code for the complete sequence? The sketchbook does not have the full sequence.
  • How to configure the PWM duty cycle?
  • What should be the Discharge timer for balancing the voltage of a cell by upto 10mV over a period of 12 hours?
  • If cell balancing is enabled for cell Cn, what will be the impact on Cn-1? If we program, say, cell 4, to be balanced, we see a drop of around 2V across the balancing resistor for that cell. In addition, we see a drop of about 17-18mV across the balancing resistor for Cell 3 also. Why?

Thanks.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.