Post Go back to editing

Unable to charge industry standard smart battery using LTC1960CG DEMO CIRCUIT 1904A

Hi,

I am trying to charge Industry standard smart battery using LTC1960CG DEMO CIRCUIT 1904A, i am successfully able to communicate with battery charger IC but unable to charge the battery.

I have implemented following procedure,

Hardware Setup:

  • DC Power supply of 15 - 20V/3.5A is given to DCin of LTC1960CG Demo Circuit 1904A
  •  Smart battery is connected to Battery 2 connector
  • MOSI, MISO, SCK and SSB pins from demo board are connected to MCU
  •  I2C lines of battery 2 are taken from P1 connector and connected to MCU
  • A Rheostat of 1k ohm resistance/150W is connected as load to DCout.

Programming:

  • Configured VDAC register.
  • Configured IDAC register.
  • Configured Charger write data to charge battery 2
  • Configured power path as Dc source
  • Periodically configuring charger write data register to avoid watchdog timer expiration
  • Reading the status of charger IC

i am unable to charge the battery using this procedure, please let me know whether the configuration which i have done is incorrect and provide a solution to charge battery.