A shorted SIMO output will not cause damage, but will cause all other SIMO channels to have unreliable output voltage regulation vs. load.
- The inductor positive ramp rate is determined only by inductor and VIN. It's not a function of VOUT in the MAX77650. A shorted output (SIMO VOUT = 0V) will not cause excessive inductor current ramp rate that violates the IP_SBB value.
- Reminder: This SIMO does not modulate inductor current to regulate output. It modulates pulse frequency. Therefore, the programmed value of IP_SBB is predictable and constant regardless of output voltage or output loading.
- The SIMO controller does not "know" that an output is shorted and will continue to give pulses.
- The shorted output will consume nearly 100% of the SIMO capacity. This deprives the other channels of capacity.
- The other SIMO outputs will still attempt to regulate output voltage, but the load regulation capability of the other outputs will become poor and unreliable due to one of the outputs being shorted.