Article What value should be used for the Current-Sense Resistor for MAX77818?

The MAX77818 FuelGauge Datasheet states that the value for the RemCapREP register is in terms of uVh. All of the capacity registers use the same scaling of 5uVh for the LSB. To scale to the measured current, a value of 10mOhm for the current-sense resistor is used. Alternately one can combine the 5uVhr and the 10mohm and use 0.5mAh for the lsb value. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.