Article MAX77734 ship mode application circuit recommendations

Figure 1, if MCU send the ship mode CMD to MAX77734, the MAX77734 can enter into the ship mode, but it will re-power on, what's the issue happened?

 

Figure 1 is the initial application schematic. When MCU send ship mode CMD to MAX77734 through I2C, MAX77734 open the Switch betweeen Vbatt and Vsys, so the Vsys will drop to "0", then the Vbuck drop to "0",  so the nEnLdo voltage is about Vbatt*4.7k/(200k+4.7k), (Vccint =Vbatt), the nEnLdo voltage is less than the  nEnLdo falling threshold voltage, so the MAX77734 think the onkey is active, then MAX77734 exit the ship mode and re-power on.
 

Figure 2 Adds a Diode between MCU's GPIO_turnon and MAX77734's nEnLdo, the issue was fixed

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.