Article If there is an overload in one of the MAX77650/MAX77651 (SIMO PMIC) outputs, will it affect other outputs?

The outputs of other channels will not be affected. Referring to SIMO Control scheme section in the MAX77650/MAX77651 datasheet, "In the event that multiple output channels need servicing at the same time, the controller ensures that no output utilizes all of the switching cycles. Instead, cycles interleave between all the outputs that are demanding service, while outputs that do not need service are skipped.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.