Article What is the maximum fast charge current of MAX77650/MAX77651?

The fast charge current of MAX77650 is programmable is from 7.5mA to 300mA by setting CHG_CC[5:0]. The sequence for setting the programmable current can be found in the MAX77650/MAX77651 Programmer's Guide and is also included below.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.