In MAX17055, AIN pin is used to determine the BST, Bi and BR bits.
If the AIN is detected, then BST = 0. If not, BST = 1.
If BST changes from 1 to 0, then Bi = 1.
If BST changes from 0 to 1, then BR = 1.
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
In MAX17055, AIN pin is used to determine the BST, Bi and BR bits.
If the AIN is detected, then BST = 0. If not, BST = 1.
If BST changes from 1 to 0, then Bi = 1.
If BST changes from 0 to 1, then BR = 1.