Article When MAX17055 is powered up from a dead battery by USB charging, the DevName is read but return value is different from value in datasheet. Why?


If MAX17055 lost power by VBATT < 2.3V, it needs VBATT > 3V to start operation. If MAX17055 is read or writen before the dead battery recovers to a high enough voltage, the operation is not reliable. The invaild DevName value means nothing, and customer should wait for the vaild DevName before other operation to MAX17055.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.