Article When the device with MAX17260 is in standby mode with very small discharge current, MAX17260 reports positive current frequently. Why?

The report current is from current ADC of MAX17260, which is actually voltage across the sense resistor. The ADC has noise in Gaussian distribution. With smaller Rsense, the output current noise will be larger. For example, Rsense=10mohm, the maximum noise current is around 6mA. However, the noise will be averaged to 0 in a long time and don't affect SOC.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.