Article Why the FullCapNom(0X23) register can be changed only through INI file and not through the App, for the MAX17260?

The FullCapNom register can be written only through dQAcc and dPAcc ratio, not directly.  If you write it directly, the FG will replace it with the calculated value from dQAcc and dPAcc at the next relax event (or immediately if the battery is already relaxed).  FullCap is also calculated every 175ms.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.