MAX77950 can work as TX. MAX77950(TX) + MAX77950(RX) should work in PeerPower mode only.
On the EVkit, we can get about 1.5W with 5V in and we can get >5W with 6V input. The limit is usually the overcurrent…
The MAX77950 PeerPower mode is not compatible with Qi, although it is similar to Qi, with the following exceptions:
No FOD support
Only Proportional parameter used for frequency control among PID…
Please note that OTP settings can only be done in the factory. V olumes needs to be very high for us to do this OTP change, and needs a strong business justification.
We recommend the following process:
Decide the Max output Power and turn off the FOD feature at the Tx device.
We recommend 7.5W, as assuming 75% efficiency, 7.5W/.75 = 10W, which can be reported…
The typical supply current would be 5mA (typ). However, with this wireless chip, the typical setup involves external FET-based connection/disconnection of the IC with the battery when wireless charging…
These are fixed thresholds built-in to the chip for thermal protection. The present chip temperature (die temperature) is tracked in the TDIE_VALUE register, which is updated periodically during chip operation…
Vrect should have ripple for proper communication. An external power supply, especially with large output capacitance, will mute this ripple and interfere with communication.