If you receive the following error when installing the software for your EVKIT
"Invalid Operation Exception: The Microsoft.ACE.OLEDB.12.0 provider is not registered in the local machine"
First remove…
Question:
How much current is going into the MAX77812 Remote Sense Input Pins (C2,C4,C5,C7,F2,F4,F5,F7). Inputs circled in red in the image below.
Answer:
Differential remote output voltage sensing…
We don't have such a design, but you can choose small receive coils from coil vendors such as Wurth, TDK and Sunlord depending on the physical dimension requirement. Adjust C to get about 100kHz resonance…