Main bias circuits are off, POR comparator is on. I2C is on when VIO is valid.
Peripheral functions (LDO, SIMO, LEDs, AMUX) do not operate in low current state because the main bias circuits are off…
A redistributable from Microsoft might be missing. Below is the link to download the Microsoft Access Database Engine Redistributable: https://www.microsoft.com/en-in/download/details.aspx?id=13255 After…
Q: Using the MAX77651 PMIC the customer might encounter an initial not working board. Why is this?
A: The PMIC has a default (OTP based) current limit of only 96mA at the charger input port. If the…
The device will wait for a wake-up signal or an I2C command to enable the main bias circuits.
This is the lowest current state of the device where the quiescent current is around ~0.3μA.