In low power consumption applications, the quiescent power consumption and standby power consumption of the power IC itself are more important. Our MAX77650 is equipped with an extremely low quiescent…
No. The default settings (the voltages that the rails reset to when power is removed) for the SIMO are one-time programmed (OTP) at the factory. They cannot be changed after that. However, the user may…
The first SIMO power supply, MAX77650/MAX77651, configures output voltage via I2C interface. Factory OTP options are also available. Therefore, the entire system size can be minimized.
For samples with…
The MAX77650 is equipped with basic protection function. For example, short-circuiting output will not damage the device. If more demanding protection is required, external protection needs to be added…
The max charge voltage of most Li+ batteries is 4.1V or 4.2V, but the battery regulation voltage of MAX77650 can be set from 3.6V to 4.6V. It also meets the low quiescent current requirement and small…
Question:
For the MAX77734, MAX77650, MAX77651, and MAX77278 linear battery charger safety timer (t FC ), what is the update condition?
Answer:
The fast-charge safety timer is intended to be set…
If the design does not utilize a hardware enable input (like a button), the pin can be strapped directly to SYS. This will make sure the part is never enabled through nEN. However, it will also make it…