In MAX17055, Timer register resolution is 175.8ms, that is when it reads 0xFFFF , 3.2Hrs time is elapsed. Whenever Timer register reaches 0xFFFF, TimerH register will increment by 1. Effectively TimerH…
The FuelGauge algorithm is agnostic to the sense resistor. The currents have units of uV/R_Sense and the capacities have units of uVh/R_Sense. When a 10 mOhm sense resistor is used, the LSB for current…
The MAX17055 can do LiSOCL2 in the same manner as the MAX17201, though since it does not have non volatile memory all the parameters need to be reloaded when the power is removed.
To interface your own board with the MAX17055 GUI, you will need the DS91230 I2C to USB adaptor. On the I2C side interface, we use a standard RJ11 connector. The pinout is shown on MAX17055 EVKIT schematics…
please see below features for ModelGauge and ModelGauge m5: • ModelGauge > ModelGauge products provides good accuracy and smallest solution size > Most cost effective > Requires characterization • ModelGauge…
There is an EZ model for Ni based batteries, but you will need to do some evaluation to see how well it works for you. If you are not satisfied with the performance, we can always do a custom model.
…
MAX17055 is equipped with Panasonic NCR model, yet the precision of this model is not as high as the common lithium-ion battery. It you need more precise measurement, the battery needs to be characterized…
There are two lower power states available in the MAX17055, hibernate mode and shutdown mode. In hibernate mode the IC consumes around 7uA of current and runs all of the normal functions of the fuel gauge…