The maximum charging current of MAX1555 is 340mA with typical charging current as 280mA when VUSB = 0 and when the DC input is active.
In the absence of a DC input, and the presence of a USB input, the maximum charging current is 100mA.
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
The maximum charging current of MAX1555 is 340mA with typical charging current as 280mA when VUSB = 0 and when the DC input is active.
In the absence of a DC input, and the presence of a USB input, the maximum charging current is 100mA.